DECENTRALIZED ROOM AUTOMATION

DISTRIBUTION BOX RAU

With our smart distribution boxes we offer you the necessary framework for your energy-efficient room automation

STUDY OF THE UNIVERSITY OF BIBERACH ON THE SUBJECT OF ENERGY SAVING 

A scientific study in three rooms with different automation levels was conducted at Biberach University of Applied Sciences during the lecture period. Considerable savings potential was identified within the process. More than 30% is possible for electrical energy consumption and even more than 50% for heating energy consumption! And all this in the existing structure without any structural changes. 

The study "Energy Efficiency through Building Automation" was conducted over a period of three years by Professor Dr.-Ing. Martin Becker and his team.

ROOM AUTOMATION INSTALLED DECENTRALLY

The areas of lighting, shading and room temperature are responsible for an optimal working atmosphere. Intelligent room automation devices are essential to ensure that they perform their task ideally. For fast, flexible and safe installation, we integrate the devices into the pluggable, decentralized electrical installation with our distribution boxes.

AREAS OF APPLICATION OF THE DISTRIBUTION BOXES RAU

Room Automation from Wieland Electric

INTELLIGENT ROOM AUTOMATION DEVICES

DISTRIBUTION BOXES - YOUR ADVANTAGES

  • Time- and resource-saving installation
  • Individual assembly
  • Room automation is placed directly in the room
  • Fuse elements directly on site
  • Future-proof - adjustments possible at any time
  • Decentralized interface between building automation levels
    • Automation level
    • Field level

SPACE FOR ANY ELECTRONICS

Covering defined areas with I/Os for automation of light, blind and room temperature.

  • Inclusion of all I/Os of a room unit
  • Supplement e.g. with power supplies
  • Support point wiring
  • Pluggable or direct connection
  • Electronics from Wieland or as extra

POWER SUPPLY

PLUGGABLE BUS CONNECTION E.G. KNX 

INTERFACE TO 
ETHERNET OR OTHER BUS SYSTEMS 

SPACE FOR YOUR ELECTRONICS

e.g. room automation controller, network technology etc.

WIELAND INSTALLATION CONNECTOR

gesis® for pluggable electrical installation

ELECTRICAL INTERFACES

Steckverbinder gesis® Classic
gesis® Connectors
Steckverbinder RST® Classic
 RST® Connectors
revos Industriesteckverbinder
revos industrial Connectors
Data connections 
Conventional introductions
Other 

SUPPORT OF THE BUS SYSTEMS COMMONLY USED IN BUILDINGS THROUGH PLUGGABLE CONNECTION OPTIONS

KNX

KNX is a uniform and manufacturer-independent communication protocol for the intelligent networking of various building automation functions, which is standardised according to EN 50090 and ISO/IEC 14543. Usually, a two-wire bus cabling is used in the building, which is plug-in wired with the gesis® NV plug-in system (type BST14, green) from Wieland.

DALI

DALI is a sub-bus system, according to IEC 62386, for lighting technology that enables 5-pole cabling with mains and signal. This is installed, for example, with the Wieland gesis® CLASSIC installation connector system (type GST18i5, pastel blue).

DALI Connector

SMI

SMI is a sub-bus system for shading technology, which enables 5-pole wiring with mains and signal. This is installed, for example, with the Wieland RST® MINI installation plug-in system (type RST16i5, turquoise blue).

SMI Connector

Ethernet oR OTHER BUS SYSTEMS

Other bus systems are common in the building and can also be plug-in integrated.

Ethernet Connector

PROCEDURE FOR YOU AS A PLANNER

What does a building installation with our products mean for you?

1. BASIC CONSIDERATION 

First of all, a few basic questions should be clarified.

  • What functions are to be integrated?
  • What electronics will be used?
  • Which room units will be controlled?
  • What construction space is available or will be needed?
  • Will the plant installation be pluggable?
2. CONSULTATION 

Contact us and arrange an appointment, during which the necessary details will be clarified. The aim of the appointment is the specification of the distribution box, the definition of the tender text and a cost estimate. 

  • Specification of electronics and internals
  • Determination of the connection type
  • Planning the distributor size and material
  • Optimization of distribution variants and quantity structures
  • Determination of accessories such as connectors or assembled cables
3. INVITING TENDERS 

They write out the distributors and accessories.

  • You receive a cost estimate from us
  • We draw up the tender texts together (neutrally as well)
  • We handle the queries from installers
4. EXECUTION 

The executing company orders the required components.

  • Appointment with your Wieland project manager
  • Creation of assembly, wiring and connection diagrams (based on AutoCAD, EPLAN)
  • Final approval of the distributors by signature of the executing company
  • Production and routine testing of the distribution boxes in accordance with the applicable standards and guidelines
  • Handover of documents and plans to the contractor

PROCESS FOR YOU AS THE EXECUTING

What changes in the installation and the process?

1. INVITING TENDERS 

You produce the cost calculation.

  • Request for a quotation from Wieland based on the invitation to tender
  • Possibly more detailed specifications
  • Preparation of a net offer, as the distribution boxes are individual customer solutions
2. FINAL DESIGN

After the contract has been awarded, you order the distributors.

  • Appointment with your Wieland project manager
  • Determination of structure and wiring in coordination
  • Optimizations based on the real conditions
  • Discussion of delivery and logistics
  • Drawings are produced by Wieland Electric
  • Release for production by customer
  • Possibly sampling
3. PRODUCTION AT WIELAND 

The manifolds are manufactured at Wieland according to the agreements.

  • Machining and, if necessary, coating of the sheet/plastic material
  • Installation and wiring of electronics or further devices with labeling of the distributors
  • Unit testing of the manifolds
4. DELIVERY

The distributors are delivered to the desired address as agreed.

  • We deliver the manifolds commissioned, together with other components
  • Delivery is made on time by forwarding agent to the desired address

OUR SMART SERVICES + SERVICES FOR YOUR SUCCESS

We support you from the planning of the project to its completion.

DISCOVER SMART SERVICES

Labeling + IDENTIFICATION

Labeling is essential for installation, commissioning and operation of the equipment. Together with you, we will develop an informative labeling concept for your distribution boxes.

Labeling of the distributors

EXAMS INDIVIDUAL AND GENERAL 

  • Unit testing according to Wieland standard
  • Function test according to agreed test plan
  • CE test on request
Exams of the distributors

DELIVERY OF THE DISTRIBUTORS

We ran your distribution boxes to the right place at the right time.

This means: Whether to you or directly to the construction site, we bring your distribution box - if necessary with cables, accessories as well as connector sets - commissioned to where they are needed.

Delivery of the Distributors

FAQ

What are the advantages of decentralized, pluggable electrical installation with distribution boxes? 
  • The Wieland solution offers simple and future-proof structures. Due to the pluggability, the systems are flexibly expandable.
  • Since the automation electronics do not have to be located in the main distribution boards, only small technical rooms are required.
  • The decentralized installation also leads to increased energy efficiency, as the three-phase current can be supplied right up to the consumer.
  • The room automation devices are located in the respective room, the fuse elements (RCCB, MCB) directly on site.
How do I get to my distribution box as an electrical planner? 

From the initial idea to tendering, awarding and execution - we design the process together with you.  Contact your responsible sales representative.

How do I get to my distribution box as an executor? 

From the tender to the final design and production at Wieland to delivery - we accompany you through the entire process. 
Contact your responsible sales representative.

How does Wieland support me with my project?

From the idea to delivery - we are always at your side.

  1. Idea: Decentralized and pluggable installation should be considered in future-oriented building planning
  2. Conceptual design: We are happy to create a concept for you, which you can present to builders or decision makers
  3. Concretization: We support you in the implementation of your concrete planning up to the cost estimation and finally to the invitation to tender
  4. Tender and offer: As soon as the tender is on the market, the interested companies receive offers from us and apply for the execution.
  5. Order: The executing company confirms the correctness of the planned distribution boxes, which then go directly to production
  6. Delivery: The desired distributors are delivered, possibly with additional picking, to the desired address as agreed.
  7. Further services: Our team is always available for you on site and in Bamberg.
Which internals can be accommodated in the distribution boxes? 

The distribution box accommodate all the necessary components for your project.

  • Room automation devices - provided by or purchased from Wieland
  • Wieland power supply and overvoltage protection
  • Terminal blocks for wiring
  • (RCCB, MCB)
  • ...
What tests are performed on the distribution boxes? 

In addition to the visual inspection and the continuity test, functional tests can also be carried out and test reports created. Furthermore, the CE marking and the conformity documents can be issued.

Our company is certified according to DIN ISO 9001 as well as EMAS.

What is the release process like? 

Release for production is based on the jointly developed and tested drawings.

From what quantity are projects accepted? 

We manufacture your distribution box from as little as 1 piece.

DOWNLOADS 

DISTRIBUTION BOXES - Brochure

0702.1 | 17 MB

Distribution Box - Smart Installation Brochure

0704.1 | 897 KB

contact

Do you need further product information?

Please contact our experts.

call: +49 951 9324 996

send request
callback service

Don’t be put on hold. 
Our experts will call you.

  1. Fill in the form
  2. Specify desired time
  3. Answer the call from our experts
arrange call