READY FOR THE REQUIREMENTS OF FUTURE-PROOF NETWORKS
WIELAND ELECTRIC SUPPORTS MAXIMUM FLEXIBILITY AND RELIABLE INDUSTRIAL COMMUNICATION WITH SFP PORTS
Faster, more flexible, more secure - the demands on network technology in the production environment are constantly increasing. The aim is to exchange even larger volumes of data quickly and reliably at the same time. In order to offer users the greatest possible flexibility in the implementation of high-performance networks, Wieland Electric has expanded its portfolio in the area of industrial communication. SFP ports for unmanaged and managed IP switches are available here, making it possible to respond quickly and easily to changing network technology requirements while also taking advantage of the benefits of fiber optic technology.
Depending on the requirements and the type of SFP module used, the SFP ports can be used to increase the number of conventional RJ45 copper-bound connections via CAT5/6/7 cable or to connect a single/multimode fiber optic cable. This means that the network technology can be designed in a highly flexible manner, for example by integrating additional network subscribers or increasing the transmission speed. This is where fiber optic technology in particular comes into its own: It makes it possible to transmit large volumes of data reliably even over long distances. In addition, because Wieland Electric's SFP ports are hot-pluggable, they can be plugged in during operation, making the switch easily adaptable. Troubleshooting is also made easier because the SFP modules can be replaced effortlessly.
As part of its portfolio expansion in the area of industrial communication, Wieland Electric enables the greatest possible flexibility in the implementation of high-performance network technology with the SFP modules