OPERATION AND VISUALIZATION IN LARGE FORMAT 

    HMI ECO TOUCH PANELS FROM WIELAND NOW ALSO AVAILABLE IN 12.1 AND 15 INCHES

     

    The HMI Eco touch panels from Wieland have grown. The powerful and robust HMI panels are now also available in 12.1 and 15 inches – to provide optimum support for sophisticated and scalable visualizations. Mechanical engineers and plant manufacturers also have the option to purchase panels with their own front design, including logo and color of their choice, to increase the prestige of their products and strengthen their spare parts business. The touch panels also allow a seamless exchange of data with both the samos Pro Compact safety controller and common PLCs.

     

    Just like the HMI Eco touch panels available in 4.3, 7, and 10 inches, which were launched back in the fall of 2018, the new 12.1 and 15-inch models are extremely robust operating devices. The screen is certified according to protection class IP66, protecting the device against strong water jets as well as any other moisture.

     

    The large HMI Eco touch panels are particularly suited to applications such as presses, large plants in the process industry, test benches, or materials processing machines with several operators working on them. Usage under extreme temperatures of -20 to +60 degrees Celsius also opens up additional fields of application such as elevators or refrigerated warehouses.

     

    Their universal interfaces and compatibility with more than 40 PLC and device manufacturers make HMI Eco touch panels very versatile. Universal interfaces for Ethernet, USB host, and USB client connections are available, along with a serial interface. The new HMI panels from Wieland are also the ideal complement to the samos Pro Compact safety controller. They enable simple visualization via the hmiPLAN software and guarantee a smooth exchange of data with the samos PLAN 6 safety software.

    PRESS CONTACT

    WIELAND ELECTRIC GMBH
    Marketing Communication
    Brennerstraße 10 – 14
    96052 Bamberg · Germany

    e-Mail

     

     

    OPERATION AND VISUALIZATION IN LARGE FORMAT_HMI_PT_2019_04.docx

    2 MB