- 20.01.2020
No tangled cables at all -Secure presentation of tablets & Co.
SOLUTIONS FOR ENERGY DISTRIBUTION IN MEDIA SHELVES
Touch it and try it out - this is how stationary trade can score points and offer the end consumer real added value. Customers particularly like to test smartphones, tablets and other small electrical appliances before buying. To do so, they must be connected to the retailer's power and data supply in a stable manner. Wieland Electric is presenting a tailor-made and above all secure plug & play solution for power distribution in media shelves and tables at the Euroshop in Düsseldorf.
Consumer electronics stores use media tables and shelves to present and demonstrate their small electrical appliances. All too often, these presentation areas are still supplied via interlinked multiple sockets - which often looks chaotic and is also prohibited. Because this type of cabling means that fuse elements can no longer be triggered safely, and there is an increased risk of fire.
This is different with the modular and pluggable system from Wieland Electric, whose components are all industrially prefabricated. Pluggable multiple sockets ensure a simple and safe power supply with a connection level according to DIN EN 61535. The connected consumers are specially protected by a fine surge protection. The pluggable components also help the dealer to save time and money. This is because both initial installation and conversion or expansion are quick, simple and flexible.
Wieland at EuroShop in Düsseldorf
You will be able to experience these and many other tailor-made solutions from Wieland Electric for the retail trade in practical terms at EuroShop from 16 to 20 February (Hall 9, Stand B 44) in Düsseldorf.