• 20.01.2020

With innovative cabling for optimal space utilization

NEW IDEAS FOR INFRASTRUCTURE CABLING IN RETAIL FROM WIELAND ELECTRIC

The refrigerated counter has to make room for the new action area, the illuminated display has to move further forward and the decoration still needs electricity - sounds elaborate? But it doesn't have to be if the smart pluggable system from Wieland Electric is used!

Retail space today must be one thing above all: flexible! Unfortunately, this flexibility all too often reaches its limits when electrical or data cables also have to be moved. At the EuroShop in Düsseldorf, Wieland Electric will show how innovative infrastructure cabling in the store can meet these new requirements. 

Completely pluggable and without junction boxes, it provides energy flexibly at any position in the sales room. Flat cables, which are routed along the walls and also in the ceiling or floor, serve as conductor rails. Lighting and cooling are supplied separately.

Temporary superstructures, decorations or secondary placements can thus be realised easily, quickly and without installation work anywhere on the surface.

Wall profiles are the solution for displays that need to be illuminated and therefore supplied with power. They are not only used for fastening, but also automatically establish the contact for the lighting when hung up.

The smart Wieland system is not only flexible, it also saves time and money thanks to its plug-in capability. Assembly times can be reduced by up to 70 per cent compared to conventional installation. Total costs are reduced by 30 percent.

Wieland at EuroShop in Düsseldorf

You will be able to experience these and many other tailor-made solutions from Wieland Electric for the retail trade in practical terms at EuroShop from 16 to 20 February (Hall 9, Stand B 44) in Düsseldorf.

 

 

DOWNLOADS

Applikation_Shop_Infrastrukturverkabelug.7z

12 MB

Press Release Infrastructure Cabeling

2 MB