• JANUARY 2025
  • PRESS INFORMATION

E-charging infrastructure easy to set up 

Wieland Electric expands electrical installation system for charging stations with new components for greater safety and flexibility

A comprehensive charging infrastructure plays a key role in the integration of electric vehicles into everyday life. There is a great need for action, especially in parking garages and underground garages. As Wieland Electric will be demonstrating at BAU 2025, there is a well thought-out complete solution for this that makes setting up an e-charging infrastructure extremely easy and ensures maximum flexibility and safety thanks to new components.

With the podis®  flat cable system from Wieland Electric, up to 20 charging stations can be connected via just one supply line. This significantly reduces the installation effort, saves material costs and minimizes the size of the required distribution cabinet. It also creates the basis for easy retrofitting of additional charging stations during the initial installation. Once the flat cable has been installed, it is sufficient to integrate a further connection module if required - a decisive advantage over conventional installation methods that saves time and money.

Convenient integration of protective devices

Wieland Electric offers a convenient solution in the form of the fuse module to meet the normative safety requirements of every final circuit. The fuse module combines the connection to the flat cable and the integration of DIN rail mounted devices. Variants with integrated FI/LS or LS are available for electromobility. As the internal wiring is prefabricated at the factory, the module only needs to be connected to the flat cable on site. With the RST® system from Wieland Electric, the outlet to the charging station can be designed to be pluggable. This eliminates the considerable installation effort that would be required with a separate, conventionally wired fuse box and outgoing cable.

In addition to the standard variants, Wieland Electric offers the option of customizing the fuse module. Based on the 5G6 or 5G16 system, four partition units offer space for the integration of completely pre-wired line, residual current, maintenance or motor-protective circuit-breakers. Various top and bottom parts allow the selection of different outputs in pluggable or conventional design with cable gland to the load. As usual with Wieland Electric, the pluggable outputs have different mechanical codings to prevent incorrect plugging and increase safety.

Even easier attachment

Time-saving and easy handling characterize the fastening of the podis® system. At BAU 2025, Wieland Electric will be showcasing a new fastening clamp for highly efficient installation. The clamp consists of just one component, with the upper and lower parts connected by a flexible plastic band. This makes handling easier and reduces the number of parts required.

Installation is time-saving with just one fixing point - only a single drill hole and therefore only one screw or nail is required. The clamp can also be closed without additional tools: The upper part is simply pressed down using a snap-in catch. Both screws and nails can be used for fastening, with the integrated HILTI geometry ensuring compatibility with HILTI setting tools. Thanks to a wide range of accessories, the new clamp can be easily mounted on mesh ducts or cable trays. In addition, the product offers a connection for pipe clamps, which enables parallel laying of pipes for data cables.

Adaptable system

Also new in the portfolio is a new module with double output, which makes it possible to operate two consumers with just one tap, thus saving one outgoing module. The module with double output can alternatively be used as a variant with an integrated top-hat rail, which has been specially designed for self-wiring. This allows components to be flexibly mounted and individually wired, making the system particularly adaptable and user-friendly.

“Whether parking garages or underground garages - with our podis® flat cable system, we not only enable user-friendly, quick and easy project planning in the field of e-charging infrastructure, but also considerable time savings during initial installation thanks to error-free and safe assembly. When it comes to expansions, the time savings are even more noticeable thanks to the high level of flexibility and simple handling,” explains Frank Nagengast, Product Information Manager at Wieland Electric.

Wieland Electric at BAU 2025
January 13 to 17, 2025
Munich Trade Fair
Hall A2 Stand 439

Image 1: Wieland Electric has added new components to its podis® system to make the installation of 
e-charging infrastructures in parking garages and underground parking lots even easier and safer

PRESS CONTACT

Daniela Kapitz
Marketing Manager Communications & PR
Phone: ++49 (951) 9324 – 291
E-Mail: daniela.kapitz@wieland-electric.com 

2025-01-wieland-en-press-bau-2025-evc.docx

117 KB